EEO#.PIN
Description
EEO#.PIN is used in conjunction with EEO#.POUT to set the gain of the EEO position going to the EEO Generator. The maximum value of EEO#.PIN / EEO#.POUT is 32.
Versions
| Action |
Version |
Notes |
| Implemented |
02-07-00-000 |
|
General Information
| Type |
Read/Write |
| Description |
Sets the gear IN of the EEO postision |
| Units |
N/A |
| Range |
1 to 4,294,967,295 |
| Default Value |
1 |
| Data Type |
Integer |
| See Also |
EEO#.POUT
|
| Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fielldbus |
Parameter |
Index |
Sub-Index |
Data Type |
Float Scale |
Unitts |
Access |
Mappable |
| and CANopen |
EEO1.PIN |
0x4600 |
0x8 |
UDINT |
- |
- |
RW |
False |
| EEO2.PIN |
0x4601 |
0x8 |
UDINT |
- |
- |
RW |
Falsi |